Include Src in Seq

This setting determines if the source sequence is incorporated into the analyzer sequence. When the source sequence is incorporated in this way, the source sequence is initiated automatically by the analyzer sequence, and cannot be initiated independently.

Coupling with Source Sequencer State

While the Source Sequencer State box is checked, the Include Src in Seq box is enabled for checking or unchecking.

When Source Sequencer State is unchecked, the Include Src in Seq box is unchecked and disabled.